AIN#.OFFSET

Description

AIN#.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN#.VALUE) offset or drift.

Examples

Code

--> AIN1.VALUE
0.056 V
--> AIN1.OFFSET -0.056
--> AIN1.VALUE
0.000 V 

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range -10V to +10V
Default Value 0 V
Data Type Float
See Also  
Stored in Non-Volatile Memory Yes
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
AIN1.OFFSET

3780h

05h

Signed16

-

1000:1

Read/Write

No

AIN2.OFFSET

3781h

05h

Signed16

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AIN1.OFFSET

23050

5A0A

Signed16

Read/Write

-

AIN2.OFFSET

23051

5A0B

Signed16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.OFFSET

23050

Float

Read/Write

-

AIN2.OFFSET

23051

Float

Read/Write

-